FlatPatternObjectDataCsys_Struct Struct¶
NXOpen.Features.FlatPattern.ObjectDataCsys is an alias for NXOpen.Features.FlatPatternObjectDataCsys_Struct
-
class
NXOpen.Features.
FlatPatternObjectDataCsys_Struct
¶ Bases:
object
Structure used to return data about objects in the flat pattern.
This structure is for points whose associativities are CSYS and Datum CSYS objects.
Fields¶
Field | Description |
---|---|
FlatPatternObject | Point in the flat pattern |
FlatSolidObject | Corresponding CSYS on the flat solid |
FormedBodyObject | Corresponding datum CSYS on the formed body |
FlatPatternObject¶
-
FlatPatternObjectDataCsys_Struct.
FlatPatternObject
¶ Point in the flat pattern
-------------------------------------
Getter Method Signature
FlatPatternObject()
Returns: Return type: NXOpen.Point
-------------------------------------
Setter Method
Signature
FlatPatternObject(value)
Parameters: value ( NXOpen.Point
) –
FlatSolidObject¶
-
FlatPatternObjectDataCsys_Struct.
FlatSolidObject
¶ Corresponding CSYS on the flat solid
-------------------------------------
Getter Method Signature
FlatSolidObject()
Returns: Return type: NXOpen.CartesianCoordinateSystem
-------------------------------------
Setter Method
Signature
FlatSolidObject(value)
Parameters: value ( NXOpen.CartesianCoordinateSystem
) –
FormedBodyObject¶
-
FlatPatternObjectDataCsys_Struct.
FormedBodyObject
¶ Corresponding datum CSYS on the formed body
-------------------------------------
Getter Method Signature
FormedBodyObject()
Returns: Return type: NXOpen.Features.DatumCsys
-------------------------------------
Setter Method
Signature
FormedBodyObject(value)
Parameters: value ( NXOpen.Features.DatumCsys
) –