FitSurfaceBuilderDirectionType Enumeration¶
NXOpen.Features.FitSurfaceBuilder.DirectionType is an alias for NXOpen.Features.FitSurfaceBuilderDirectionType
-
class
NXOpen.Features.
FitSurfaceBuilderDirectionType
¶ Bases:
object
Direction method provides the ability to specify the projection direction and orientation
Enum Members
Enum Member Enum Member Description BestFit The fit target is sort of rectangular. Vector Vector will specify the fit direction. Orientation Orientation will specify the direction and U/V orientation. Csys CSYS will specify same as orientation but with the need to make it associative with existing geometry. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-