EmbeddedOperationBuilder Class¶
-
class
NXOpen.Features.
EmbeddedOperationBuilder
¶ Bases:
NXOpen.Builder
Represents an EmbeddedOperationBuilder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitOperation | Commits the operation and creates the feature. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOperation | Returns the feature currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CommitOperation¶
-
EmbeddedOperationBuilder.
CommitOperation
¶ Commits the operation and creates the feature.
If it’s for a recipe curve of Drafting sketch, there will be no feature returned because Drafting sketch is featureless.
Signature
CommitOperation()
Returns: Return type: NXOpen.Features.Feature
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetOperation¶
-
EmbeddedOperationBuilder.
GetOperation
¶ Returns the feature currently being edited by this builder.
If a new feature is being created, and the builder has not yet been commited, returns None.
Signature
GetOperation()
Returns: Return type: NXOpen.Features.Feature
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
EmbeddedOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.