EdgeBlendBuilderOverlap Enumeration¶
NXOpen.Features.EdgeBlendBuilder.Overlap is an alias for NXOpen.Features.EdgeBlendBuilderOverlap
-
class
NXOpen.Features.
EdgeBlendBuilderOverlap
¶ Bases:
object
This enum represents the Overlap resolution options for Edge Blend
Enum Members
Enum Member Enum Member Description MaintainAndIntersect Maintain Blend and IntersectDifferentConvexityRollOver If different convexity,roll overAnyConvexityRollOver Any convexity,roll over-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-