DraftBodyBuilderRepairOption Enumeration¶
NXOpen.Features.DraftBodyBuilder.RepairOption is an alias for NXOpen.Features.DraftBodyBuilderRepairOption
-
class
NXOpen.Features.
DraftBodyBuilderRepairOption
¶ Bases:
object
Describes the different repair options.
Enum Members
Enum Member Enum Member Description None No repair option is specifiedBlends Repair concave miter corners with blendsPlanes Repair concave miter corners with planesBoth Repair concave miter corners with both blends and planes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-