DraftBodyBuilderMatchOption Enumeration¶
NXOpen.Features.DraftBodyBuilder.MatchOption is an alias for NXOpen.Features.DraftBodyBuilderMatchOption
-
class
NXOpen.Features.
DraftBodyBuilderMatchOption
¶ Bases:
object
Describes the different match options.
Enum Members
Enum Member Enum Member Description None No match option is specifiedAll All faces-to-draft are to be matchedAllButSelected All faces-to-draft except the ones explicitly indicated are to be matched-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-