DatumPlaneBuilderConstraintType Enumeration¶
NXOpen.Features.DatumPlaneBuilder.ConstraintType is an alias for NXOpen.Features.DatumPlaneBuilderConstraintType
-
class
NXOpen.Features.
DatumPlaneBuilderConstraintType
¶ Bases:
object
Specifies different constraint types of selected geometries
Enum Members
Enum Member Enum Member Description Undefined Not definedCoincident Coincident constraintParallel Parallel constraintPerpendicular Perpendicular constraintCenter Center constraintTangent Tangent constraintDistance Distance constraintAngle Angle constraintFrenet Frenet constraint-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-