DatumAxisBuilderTypes Enumeration¶
NXOpen.Features.DatumAxisBuilder.Types is an alias for NXOpen.Features.DatumAxisBuilderTypes
-
class
NXOpen.Features.
DatumAxisBuilderTypes
¶ Bases:
object
New Datum Axis types in NX5
Enum Members
Enum Member Enum Member Description Inferred InferredIntersection Datum axis at the intersection of objectsCurveOrFaceAxis Datum axis at the curve or face axisOnCurveVector Datum axis at vector on curveXcAxis Datum axis thru X axisYcAxis Datum axis thru Y axisZcAxis Datum axis thru Z axisPointAndDir Datum axis thru a point and parallel or perpendicular to directionTwoPoints Datum axis thru two pointFixed Indicate the datum axis is fixed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-