CircularBlendCurveBuilderCylinderRadiusOption Enumeration¶
NXOpen.Features.CircularBlendCurveBuilder.CylinderRadiusOption is an alias for NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
-
class
NXOpen.Features.
CircularBlendCurveBuilderCylinderRadiusOption
¶ Bases:
object
Represents the cylinder radius options
Enum Members
Enum Member Enum Member Description PointOnFirstCurve Radius by point on first curvePointOnSecondCurve Radius by point on second curveValue Radius by value-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-