BridgeCurveBuilderExShapeControlMethods Enumeration¶
NXOpen.Features.BridgeCurveBuilderEx.ShapeControlMethods is an alias for NXOpen.Features.BridgeCurveBuilderExShapeControlMethods
-
class
NXOpen.Features.
BridgeCurveBuilderExShapeControlMethods
¶ Bases:
object
Shape control methods
Enum Members
Enum Member Enum Member Description TangentMagnitude Shape using tangent magnitude at endsDepthSkew Shape using depth and skew valueConic Shape using rho value of a conic. Valid only when end sections are coplanar.TemplateCurve Shape by a template curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-