AssociativityType Enumeration¶
-
class
NXOpen.Features.
AssociativityType
¶ Bases:
object
Represents the associativity type for a dimension entity Enum Members
Enum Member Enum Member Description EndPoint End-point (determined from 3d help point)ArcCenter Arc-centerTangency TangencyEndPoint1 1st end point (at minimum parameter value)EndPoint2 2nd end pointVerticalCenterline1 vertical centerline end point 1VerticalCenterline2 vertical centerline end point 2HorizontalCenterline1 horizontal centerline end point 1HorizontalCenterline2 horizontal centerline end point 2-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-