AnalyzePocketBuilderToolTypes Enumeration¶
NXOpen.Features.AnalyzePocketBuilder.ToolTypes is an alias for NXOpen.Features.AnalyzePocketBuilderToolTypes
-
class
NXOpen.Features.
AnalyzePocketBuilderToolTypes
¶ Bases:
object
Represents the tool type which defines how the angled walls are cut.
Enum Members
Enum Member Enum Member Description Unknown unknown.EndMill End Mill.TCutter T Cutter.SphericalMill Spherical Mill.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-