AestheticFaceBlendBuilderStartTrimObjectType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.StartTrimObjectType is an alias for NXOpen.Features.AestheticFaceBlendBuilderStartTrimObjectType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderStartTrimObjectType
¶ Bases:
object
Start object overriding trim options
Enum Members
Enum Member Enum Member Description None Does not override start trim object.Plane Overrides start trim object with plane.Face Override start trim object with face.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-