AestheticFaceBlendBuilderSegmentationType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.SegmentationType is an alias for NXOpen.Features.AestheticFaceBlendBuilderSegmentationType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderSegmentationType
¶ Bases:
object
Segmentations options
Enum Members
Enum Member Enum Member Description AtAllTransitions Segmentation at all transitionsAtTransitionsonFaceChain1 Segmentation at Face Chain1 transitionAtTransitionsonFaceChain2 Segementation at Face Chain2 transitionAtAllTransitionsandMergeSmallBlendFaces Secgmentation at all transitions and merge small blend faces-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-