FaceFaceType Enumeration¶
NXOpen.Face.FaceType is an alias for NXOpen.FaceFaceType
-
class
NXOpen.
FaceFaceType
¶ Bases:
object
Solid face type.
Enum Members
Enum Member Enum Member Description Rubber Rubber face, no surface attachedPlanar Planar faceCylindrical Cylindrical faceConical Conical faceSpherical Spherical faceSurfaceOfRevolution Face from surface of revolutionParametric Parametric faceBlending Blending faceOffset Offset faceSwept Swept faceUndefined Undefined face type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-