ExtrudeOffsetDataOffsetType Enumeration¶
-
class
NXOpen.
ExtrudeOffsetDataOffsetType
¶ Bases:
object
This enum represents the type of offset Enum Members
Enum Member Enum Member Description None No offsetNormalOffset Offset with two different distancesSymmetricOffset Offset with same distance in both directionsSingleOffset Offset with single distance in one direction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-