ExpressionGroupCollection Class¶
-
class
NXOpen.
ExpressionGroupCollection
¶ Bases:
object
Represents a collection of expressions groups.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CheckName | Returns whether or not expression group name is valid. |
Create | Creates an expression group @return the new expression group |
Delete | Deletes an array of one or more expression groups. |
ExportExpressionGroupsToFile | Exports the expressions in an expression group to a text file, or, if ‘file_name’ is None, list the expressions in the listing window. |
FindObject | Finds the NXOpen.ExpressionGroup with the given identifier as recorded in a journal. |
GetAllExpressionGroupsInPart | Returns an array of all expression groups in a part . |
GetDefault | Return the default expression group @return the default expression group |
GetGroupOfExpression | Returns expression group owner of an expression. |
SetAllGroupsVisible | Make all expression groups visible |
Property Detail¶
Active¶
-
ExpressionGroupCollection.
Active
¶ Returns or sets the active expression group
-------------------------------------
Getter Method
Signature
Active()
Returns: the active expression group Return type: NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Active(expressionGroup)
Parameters: expressionGroup ( NXOpen.ExpressionGroup
) – the expression group to make activeNew in version NX10.0.0.
License requirements: None.
Method Detail¶
CheckName¶
-
ExpressionGroupCollection.
CheckName
¶ Returns whether or not expression group name is valid.
Signature
CheckName(name)
Parameters: name (str) – the name of the expression group to check. Returns: the status of the name check. True if name is okay Return type: bool New in version NX10.0.0.
License requirements: None.
Create¶
-
ExpressionGroupCollection.
Create
¶ Creates an expression group
Signature
Create(name)
Parameters: name (str) – the name for the expression group. Returns: the new expression group Return type: NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.
Delete¶
-
ExpressionGroupCollection.
Delete
¶ Deletes an array of one or more expression groups.
This method should be used when deleting an Expression group. DO NOT use the delete methods in Update.ja to delete expression groups
Signature
Delete(expressionGroup)
Parameters: expressionGroup (list of NXOpen.ExpressionGroup
) – array of expression groups to deleteNew in version NX10.0.0.
License requirements: None.
ExportExpressionGroupsToFile¶
-
ExpressionGroupCollection.
ExportExpressionGroupsToFile
¶ Exports the expressions in an expression group to a text file, or, if ‘file_name’ is None, list the expressions in the listing window.
Throws an exception if there is any error.
NOTE: if the file already exists, an exception is thrown and the file is not overwritten.
Signature
ExportExpressionGroupsToFile(expressionGroups, fileName, sortType)
Parameters: - expressionGroups (list of
NXOpen.ExpressionGroup
) – - fileName (str) – File name specification to export expressions into.
- sortType (
NXOpen.ExpressionCollectionSortType
) – How to sort the exported expressions
New in version NX10.0.0.
License requirements: None.
- expressionGroups (list of
FindObject¶
-
ExpressionGroupCollection.
FindObject
¶ Finds the
NXOpen.ExpressionGroup
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Expression found Return type: NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.
GetAllExpressionGroupsInPart¶
-
ExpressionGroupCollection.
GetAllExpressionGroupsInPart
¶ Returns an array of all expression groups in a part .
Signature
GetAllExpressionGroupsInPart()
Returns: array of groupsexpression groups Return type: list of NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.
GetDefault¶
-
ExpressionGroupCollection.
GetDefault
¶ Return the default expression group
Signature
GetDefault()
Returns: the default expression group Return type: NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.
GetGroupOfExpression¶
-
ExpressionGroupCollection.
GetGroupOfExpression
¶ Returns expression group “owner” of an expression.
Signature
GetGroupOfExpression(expression)
Parameters: expression ( NXOpen.Expression
) – the expression to queryReturns: expression group of expression Return type: NXOpen.ExpressionGroup
New in version NX10.0.0.
License requirements: None.