EdgeEdgeType Enumeration¶
NXOpen.Edge.EdgeType is an alias for NXOpen.EdgeEdgeType
-
class
NXOpen.
EdgeEdgeType
¶ Bases:
object
Solid edge type.
Enum Members
Enum Member Enum Member Description Rubber Rubber edge, no curve attachedLinear Linear edgeCircular Circular edgeElliptical Elliptical edgeIntersection Intersection edgeSpline Spline edgeSpCurve SP curve edgeForeign Foreign edgeConstantParameter Constant parameter edgeTrimmedCurve Trimmed curve edgeUndefined Undefined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-