DxfdwgCreatorAutoCADRevisionOptions Enumeration¶
NXOpen.DxfdwgCreator.AutoCADRevisionOptions is an alias for NXOpen.DxfdwgCreatorAutoCADRevisionOptions
-
class
NXOpen.
DxfdwgCreatorAutoCADRevisionOptions
¶ Bases:
object
AutoCad Revision option
Enum Members
Enum Member Enum Member Description R2000 output autocad version 2000R2004 output autocad version 2004R2005 output autocad version 2005R2007 output autocad version 2007R2010 output autocad version 2010R2013 output autocad version 2013-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-