VirtualIntersectionsViewStyle Class¶
-
class
NXOpen.Drawings.
VirtualIntersectionsViewStyle
¶ Bases:
object
Represents set of Virtual Intersections View Style Preferences applicable to drafting views.
Allows to display imaginary intersection curves.
To obtain an instance of this class use
Drawings.ViewStyle.VirtualIntersections
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AdjacentBlends | Returns or sets the status of adjacent blends. |
AdjacentBlendsColor | Returns or sets the color of adjacent blends. |
AdjacentBlendsEndGaps | Returns or sets the status of adjacent blends end gaps. |
AdjacentBlendsEndGapsData | Returns or sets the value of adjacent blends end gaps. |
AdjacentBlendsFont | Returns or sets the font of adjacent blends. |
AdjacentBlendsWidth | Returns or sets the width of adjacent blends. |
VirtualIntersection | Returns or sets the status of virtual intersection. |
Methods¶
Property Detail¶
AdjacentBlends¶
-
VirtualIntersectionsViewStyle.
AdjacentBlends
¶ Returns or sets the status of adjacent blends.
-------------------------------------
Getter Method
Signature
AdjacentBlends()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlends(adjacentBlends)
Parameters: adjacentBlends (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
AdjacentBlendsColor¶
-
VirtualIntersectionsViewStyle.
AdjacentBlendsColor
¶ Returns or sets the color of adjacent blends.
The value should be between 1 and 216.
-------------------------------------
Getter Method
Signature
AdjacentBlendsColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlendsColor(adjacentBlendsColor)
Parameters: adjacentBlendsColor (int) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
AdjacentBlendsEndGaps¶
-
VirtualIntersectionsViewStyle.
AdjacentBlendsEndGaps
¶ Returns or sets the status of adjacent blends end gaps.
It controls the display of visible ends. If True, the visible ends are suppressed from the display. The length of the suppressed end is in drawing units and is controlled by the value set in the End Gap field. If False, the visible ends are not suppressed from the display.
-------------------------------------
Getter Method
Signature
AdjacentBlendsEndGaps()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlendsEndGaps(adjacentBlendsEndGaps)
Parameters: adjacentBlendsEndGaps (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
AdjacentBlendsEndGapsData¶
-
VirtualIntersectionsViewStyle.
AdjacentBlendsEndGapsData
¶ Returns or sets the value of adjacent blends end gaps.
-------------------------------------
Getter Method
Signature
AdjacentBlendsEndGapsData()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlendsEndGapsData(adjacentBlendsEndGapsData)
Parameters: adjacentBlendsEndGapsData (float) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
AdjacentBlendsFont¶
-
VirtualIntersectionsViewStyle.
AdjacentBlendsFont
¶ Returns or sets the font of adjacent blends.
-------------------------------------
Getter Method
Signature
AdjacentBlendsFont()
Returns: Return type: NXOpen.Preferences.Font
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlendsFont(adjacentBlendsFont)
Parameters: adjacentBlendsFont ( NXOpen.Preferences.Font
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
AdjacentBlendsWidth¶
-
VirtualIntersectionsViewStyle.
AdjacentBlendsWidth
¶ Returns or sets the width of adjacent blends.
-------------------------------------
Getter Method
Signature
AdjacentBlendsWidth()
Returns: Return type: NXOpen.Preferences.Width
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlendsWidth(adjacentBlendsWidth)
Parameters: adjacentBlendsWidth ( NXOpen.Preferences.Width
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VirtualIntersection¶
-
VirtualIntersectionsViewStyle.
VirtualIntersection
¶ Returns or sets the status of virtual intersection.
-------------------------------------
Getter Method
Signature
VirtualIntersection()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VirtualIntersection(virtualIntersection)
Parameters: virtualIntersection (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)