ViewStyleShadingBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleShadingBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SHADING tab on the View Style Dialog (Drawings.
ViewStyleShadingBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance data on the SHADING tab of the View Style Dialog |
CutFaceColor | Returns or sets the cut face color on the SHADING tab of the View Style Dialog |
EdgeTolerance | Returns or sets the edge tolerance data on the SHADING tab of the View Style Dialog |
FaceTolerance | Returns or sets the face tolerance data on the SHADING tab of the View Style Dialog |
HiddenWireframeColor | Returns or sets the hidden wireframe color on the SHADING tab of the View Style Dialog |
RenderingStyle | Returns or sets the rendering style option on the SHADING tab of the View Style Dialog |
ShadeTolerance | Returns or sets the shade tolerance option on the SHADING tab of the View Style Dialog |
ShininessScale | Returns or sets the shininess scale data on the SHADING tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
TwoSidedLight | Returns or sets the two sided light toggle on the SHADING tab of the View Style Dialog |
VisibleWireframeColor | Returns or sets the visible wireframe color on the SHADING tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
ViewStyleShadingBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Returns the angle tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleToleranceData)
Parameters: angleToleranceData (float) – Sets a new angle tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CutFaceColor¶
-
ViewStyleShadingBuilder.
CutFaceColor
¶ Returns or sets the cut face color on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
CutFaceColor()
Returns: Returns the cut face color that is on the shading sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutFaceColor(cutFaceColor)
Parameters: cutFaceColor (Id) – Sets a new cut face color on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EdgeTolerance¶
-
ViewStyleShadingBuilder.
EdgeTolerance
¶ Returns or sets the edge tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EdgeTolerance()
Returns: Returns the edge tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeTolerance(edgeToleranceData)
Parameters: edgeToleranceData (float) – Sets a new edge tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FaceTolerance¶
-
ViewStyleShadingBuilder.
FaceTolerance
¶ Returns or sets the face tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
FaceTolerance()
Returns: Returns the face tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceTolerance(faceToleranceData)
Parameters: faceToleranceData (float) – Sets a new face tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
RenderingStyle¶
-
ViewStyleShadingBuilder.
RenderingStyle
¶ Returns or sets the rendering style option on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
RenderingStyle()
Returns: Returns the rendering style option that is on the shading sub-builder Return type: NXOpen.Preferences.ShadingRenderingStyleOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenderingStyle(renderingStyleOption)
Parameters: renderingStyleOption ( NXOpen.Preferences.ShadingRenderingStyleOption
) – Sets a new rendering style option on the shading sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ShadeTolerance¶
-
ViewStyleShadingBuilder.
ShadeTolerance
¶ Returns or sets the shade tolerance option on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ShadeTolerance()
Returns: Returns the shade tolerance option that is on the shading sub-builder Return type: NXOpen.Preferences.ShadingToleranceOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadeTolerance(shadeToleranceOption)
Parameters: shadeToleranceOption ( NXOpen.Preferences.ShadingToleranceOption
) – Sets a new shade tolerance option on the shading sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ShininessScale¶
-
ViewStyleShadingBuilder.
ShininessScale
¶ Returns or sets the shininess scale data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ShininessScale()
Returns: Returns the shininess scale that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShininessScale(shininessScaleData)
Parameters: shininessScaleData (float) – Sets a new shininess scale on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
TwoSidedLight¶
-
ViewStyleShadingBuilder.
TwoSidedLight
¶ Returns or sets the two sided light toggle on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
TwoSidedLight()
Returns: Returns the two sided light toggle value that is on the shading sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwoSidedLight(twoSidedLightToggle)
Parameters: twoSidedLightToggle (bool) – Sets a new two sided light toggle value on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
VisibleWireframeColor¶
-
ViewStyleShadingBuilder.
VisibleWireframeColor
¶ Returns or sets the visible wireframe color on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
VisibleWireframeColor()
Returns: Returns the visible wireframe color that is on the shading sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleWireframeColor(visibleWireframeColor)
Parameters: visibleWireframeColor (Id) – Sets a new visible wireframe color on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleShadingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.