ViewStyleSectionBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleSectionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SECTION tab on the View Style Dialog (Drawings.
ViewStyleSectionBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdjacencyToleranceData | Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog |
AssemblyTolerance | Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog |
Background | Returns or sets the background toggle on the SECTION tab of the View Style Dialog |
Bendlines | Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog |
Crosshatch | Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog |
DisplaySectionLine | Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog |
Foreground | Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog |
HiddenLineHatching | Returns or sets the hidden line hatching toggle on the SECTION tab of the View Style Dialog |
RestrictCrosshatchAngle | Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog |
SheetBodies | Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdjacencyToleranceData¶
-
ViewStyleSectionBuilder.
AdjacencyToleranceData
¶ Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AdjacencyToleranceData()
Returns: Returns the assembly tolerance that is on the section sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacencyToleranceData(adjacencyToleranceData)
Parameters: adjacencyToleranceData (float) – Sets a new assembly tolerance on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
AssemblyTolerance¶
-
ViewStyleSectionBuilder.
AssemblyTolerance
¶ Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AssemblyTolerance()
Returns: Returns the assembly tolerance toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssemblyTolerance(assemblyToleranceToggle)
Parameters: assemblyToleranceToggle (bool) – Sets a new assembly tolerance toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Background¶
-
ViewStyleSectionBuilder.
Background
¶ Returns or sets the background toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Background()
Returns: Returns the background toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Background(backgroundToggle)
Parameters: backgroundToggle (bool) – Sets a new background toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Bendlines¶
-
ViewStyleSectionBuilder.
Bendlines
¶ Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Bendlines()
Returns: Returns the bendlines toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Bendlines(bendlinesToggle)
Parameters: bendlinesToggle (bool) – Sets a new bendlines toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Crosshatch¶
-
ViewStyleSectionBuilder.
Crosshatch
¶ Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Crosshatch()
Returns: Returns the crosshatch toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Crosshatch(crosshatchToggle)
Parameters: crosshatchToggle (bool) – Sets a new crosshatch toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
DisplaySectionLine¶
-
ViewStyleSectionBuilder.
DisplaySectionLine
¶ Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
DisplaySectionLine()
Returns: Returns the display section line toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySectionLine(displaySectionLine)
Parameters: displaySectionLine (bool) – Sets a new display section line toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Foreground¶
-
ViewStyleSectionBuilder.
Foreground
¶ Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Foreground()
Returns: Returns the foreground toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Foreground(foregroundToggle)
Parameters: foregroundToggle (bool) – Sets a new foreground toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
RestrictCrosshatchAngle¶
-
ViewStyleSectionBuilder.
RestrictCrosshatchAngle
¶ Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
RestrictCrosshatchAngle()
Returns: Returns the restrict crosshatch angle toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RestrictCrosshatchAngle(restrictCrosshatchAngleToggle)
Parameters: restrictCrosshatchAngleToggle (bool) – Sets a new restrict crosshatch angle toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SheetBodies¶
-
ViewStyleSectionBuilder.
SheetBodies
¶ Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SheetBodies()
Returns: Returns the sheet bodies toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SheetBodies(sheetBodiesToggle)
Parameters: sheetBodiesToggle (bool) – Sets a new sheet bodies toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.