ViewStyleFPCalloutsBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleFPCalloutsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings.
ViewStyleFPCalloutsBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
State | Returns or sets the state toggle on the Callout section of the Flat Pattern tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Type | Returns the type of Flat Pattern Callout |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
State¶
-
ViewStyleFPCalloutsBuilder.
State
¶ Returns or sets the state toggle on the Callout section of the Flat Pattern tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
State()
Returns: Returns the state toggle value that is on the callout section of the flat pattern sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
State(stateToggle)
Parameters: stateToggle (bool) – Sets a new state toggle value on the callout section of the flat pattern sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleFPCalloutsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.