ViewScaleBuilderType Enumeration¶
NXOpen.Drawings.ViewScaleBuilder.Type is an alias for NXOpen.Drawings.ViewScaleBuilderType
-
class
NXOpen.Drawings.
ViewScaleBuilderType
¶ Bases:
object
The view scale type
Enum Members
Enum Member Enum Member Description Ratio determine scale from numerator / denominatorExpression determine scale from expression-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-