ViewOrientationBuilderOrientation Enumeration¶
NXOpen.Drawings.ViewOrientationBuilder.Orientation is an alias for NXOpen.Drawings.ViewOrientationBuilderOrientation
-
class
NXOpen.Drawings.
ViewOrientationBuilderOrientation
¶ Bases:
object
This enum represents view orientation type.
Drawings.ViewOrientationBuilderOrientation.InheritOrientation
andDrawings.ViewOrientationBuilderOrientation.SectionExisting
options require a view selection.Enum Members
Enum Member Enum Member Description Orthographic OrthographicInheritOrientation Inherit Orientation from a ViewUseParentOrientation Use Parent View OrientationUseParentOrienation DO NOT USE Deprecated as of NX75SectionExisting Section an Existing View-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-