SvtBuilder Class¶
-
class
NXOpen.Drawings.
SvtBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.SvtBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BackgroundFaces | Returns the background faces that are to be shown in the section view. |
NormalDirection | Returns or sets the vector that represents the normal direction for the view to be created or edited. |
Orientation | Returns or sets the orientation flag that indicates whether or not the Section View Tool view should be used to orient the section view when it is placed |
Tag | Returns the Tag for this object. |
XDirection | Returns or sets the x direction vector for the view to be created or edited. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BackgroundFaces¶
-
SvtBuilder.
BackgroundFaces
¶ Returns the background faces that are to be shown in the section view.
When none are selected, all faces will be shown
-------------------------------------
Getter Method
Signature
BackgroundFaces()
Returns: Return type: NXOpen.SelectFaceList
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
NormalDirection¶
-
SvtBuilder.
NormalDirection
¶ Returns or sets the vector that represents the normal direction for the view to be created or edited.
The vector is used only if the Orientation flag is on. The purpose of the direction vectors is make a simple, simulated pictorial view. Consequently it is expected that a desireable orientation will need to be found interactive using the tool, and that specification by vectors will be of marginal use. The ability to specifiy the orientation is being included only for completeness.
-------------------------------------
Getter Method
Signature
NormalDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
NormalDirection(normalDirection)
Parameters: normalDirection ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Orientation¶
-
SvtBuilder.
Orientation
¶ Returns or sets the orientation flag that indicates whether or not the Section View Tool view should be used to orient the section view when it is placed
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: bool New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation (bool) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
XDirection¶
-
SvtBuilder.
XDirection
¶ Returns or sets the x direction vector for the view to be created or edited.
The vector is used only if the Orientation flag is on. The purpose of the direction vectors is make a simple, simulated pictorial view. Consequently it is expected that a desireable orientation will need to be found interactive using the tool, and that specification by vectors will be of marginal use. The ability to specifiy the orientation is being included only for completeness.
-------------------------------------
Getter Method
Signature
XDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
XDirection(xDirection)
Parameters: xDirection ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
SvtBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.