SheetTemplateManager Class¶
-
class
NXOpen.Drawings.
SheetTemplateManager
¶ Bases:
object
Represents a manager of :py:class:`NXOpen.Drawings.DraftingView`s.
To obtain an instance of this class, refer to
NXOpen.Drawings.DrawingSheetCollection
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates drawings via the sheet template, given a path to sheet template |
Method Detail¶
Create¶
-
SheetTemplateManager.
Create
¶ Creates drawings via the sheet template, given a path to sheet template
Signature
Create(pathToPartName)
Parameters: pathToPartName (str) – Part name of sheet template NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)