DrawingSheetStandardSheetSize Enumeration¶
NXOpen.Drawings.DrawingSheet.StandardSheetSize is an alias for NXOpen.Drawings.DrawingSheetStandardSheetSize
-
class
NXOpen.Drawings.
DrawingSheetStandardSheetSize
¶ Bases:
object
Standard Drawing sizes
Enum Members
Enum Member Enum Member Description A 8.5 x 11 inchesB 11 X 17 inchesC 17 X 22 inchesD 22 X 34 inchesE 34 X 44 inchesF 28 X 40 inchesH 28 X 44 inchesJ 34 X 55 inchesA0 841 x 1189 millimetersA1 594 X 841 millimetersA2 420 X 594 millimetersA3 297 X 420 millimetersA4 210 X 297 millimeters-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-