DrawingRegionCollection Class¶
-
class
NXOpen.Drawings.
DrawingRegionCollection
¶ Bases:
object
Represents a collection of drawing regions
Use
NXOpen.Drawings.DrawingRegion
to get the instance of this class.New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateAddObjectsToRegionBuilder | Creates add objects to region builder @return |
CreateDrawingRegionBuilder | Creates the DrawingRegion builder @return |
CreateRemoveObjectsBuilder | Creates remove objects builder @return |
CreateSelectRegionBuilder | Creates select region builder @return |
FindObject | Finds the NXOpen.Drawings.DrawingRegion with the given name. |
Method Detail¶
CreateAddObjectsToRegionBuilder¶
-
DrawingRegionCollection.
CreateAddObjectsToRegionBuilder
¶ Creates add objects to region builder
Signature
CreateAddObjectsToRegionBuilder()
Returns: Return type: NXOpen.Drawings.AddObjectsToRegionBuilder
New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
CreateDrawingRegionBuilder¶
-
DrawingRegionCollection.
CreateDrawingRegionBuilder
¶ Creates the DrawingRegion builder
Signature
CreateDrawingRegionBuilder(object)
Parameters: object ( NXOpen.Drawings.DrawingRegion
) –Returns: Return type: NXOpen.Drawings.DrawingRegionBuilder
New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
CreateRemoveObjectsBuilder¶
-
DrawingRegionCollection.
CreateRemoveObjectsBuilder
¶ Creates remove objects builder
Signature
CreateRemoveObjectsBuilder()
Returns: Return type: NXOpen.Drawings.RemoveObjectsBuilder
New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
CreateSelectRegionBuilder¶
-
DrawingRegionCollection.
CreateSelectRegionBuilder
¶ Creates select region builder
Signature
CreateSelectRegionBuilder()
Returns: Return type: NXOpen.Drawings.SelectRegionBuilder
New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
FindObject¶
-
DrawingRegionCollection.
FindObject
¶ Finds the
NXOpen.Drawings.DrawingRegion
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Region name Returns: Drawing Region object Return type: NXOpen.Drawings.DrawingRegion
New in version NX8.0.0.
License requirements: None.