DrawingRegionBuilderRegionGrowthDirection Enumeration¶
NXOpen.Drawings.DrawingRegionBuilder.RegionGrowthDirection is an alias for NXOpen.Drawings.DrawingRegionBuilderRegionGrowthDirection
-
class
NXOpen.Drawings.
DrawingRegionBuilderRegionGrowthDirection
¶ Bases:
object
Specifies the region growth direction (this is for
NXOpen.Annotations.CustomSymbol
andNXOpen.Annotations.Note
)Enum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “RightfromTopLeft”, ” - ” “RightfromBottomLeft”, ” - ” “LeftfromTopRight”, ” - ” “LeftfromBottomRight”, ” - ” “DownfromTopLeft”, ” - ” “DownfromTopRight”, ” - ” “UpfromBottomLeft”, ” - ” “UpfromBottomRight”, ” - ” “None”, ” - “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.