DrawingFormatSheetBuilder Class¶
-
class
NXOpen.Drawings.
DrawingFormatSheetBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.DrawingFormatSheetBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
InitialSecondarySheetNumber | Returns or sets the initial secondary sheet number |
InitialSheetNumber | Returns or sets the initial sheet number |
SecondaryNumberDelimiter | Returns or sets the secondary number delimiter |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InitialSecondarySheetNumber¶
-
DrawingFormatSheetBuilder.
InitialSecondarySheetNumber
¶ Returns or sets the initial secondary sheet number
-------------------------------------
Getter Method
Signature
InitialSecondarySheetNumber()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialSecondarySheetNumber(initialSecondarySheetNumber)
Parameters: initialSecondarySheetNumber (str) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InitialSheetNumber¶
-
DrawingFormatSheetBuilder.
InitialSheetNumber
¶ Returns or sets the initial sheet number
-------------------------------------
Getter Method
Signature
InitialSheetNumber()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialSheetNumber(initialSheetNumber)
Parameters: initialSheetNumber (str) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SecondaryNumberDelimiter¶
-
DrawingFormatSheetBuilder.
SecondaryNumberDelimiter
¶ Returns or sets the secondary number delimiter
-------------------------------------
Getter Method
Signature
SecondaryNumberDelimiter()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondaryNumberDelimiter(secondaryNumberDelimiter)
Parameters: secondaryNumberDelimiter (str) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DrawingFormatSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.