DraftingCurveCollection Class¶
-
class
NXOpen.Drawings.
DraftingCurveCollection
¶ Bases:
object
Represents a collection of :py:class:`NXOpen.Drawings.DraftingCurve`s.
To obtain an instance of this class, refer to
NXOpen.Drawings.DraftingBody
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Drawings.DraftingCurve with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
DraftingCurveCollection.
FindObject
¶ Finds the
NXOpen.Drawings.DraftingCurve
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the DraftingCurve to be found Returns: DraftingCurve with this identifier Return type: NXOpen.Drawings.DraftingCurve
New in version NX8.5.0.
License requirements: None.