DetailViewBuilderLabelOnParentType Enumeration¶
NXOpen.Drawings.DetailViewBuilder.LabelOnParentType is an alias for NXOpen.Drawings.DetailViewBuilderLabelOnParentType
-
class
NXOpen.Drawings.
DetailViewBuilderLabelOnParentType
¶ Bases:
object
the display type for the label on parent
Enum Members
Enum Member Enum Member Description None No displayCircle CircularNote Circular with a noteLabel Circular with a labelEmbedded Circular with a note embeddedBoundary The shape is the same as the boundary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-