BordersAndZonesCollection Class¶
-
class
NXOpen.Drawings.
BordersAndZonesCollection
¶ Bases:
object
Represents a collection of
NXOpen.Drawings.BordersAndZones
objectsTo obtain an instance of this class, refer to
NXOpen.DraftingManager
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateBordersAndZonesBuilder | Creates a borders and zones builder @return BordersAndZonesBuilder object |
FindObject | Finds the NXOpen.Drawings.BordersAndZones with the given name. |
Method Detail¶
CreateBordersAndZonesBuilder¶
-
BordersAndZonesCollection.
CreateBordersAndZonesBuilder
¶ Creates a borders and zones builder
Signature
CreateBordersAndZonesBuilder(bordersAndZones)
Parameters: bordersAndZones ( NXOpen.Drawings.BordersAndZones
) –NXOpen.Drawings.BordersAndZones
to be redefined, if None then creates a new oneReturns: BordersAndZonesBuilder object Return type: NXOpen.Drawings.BordersAndZonesBuilder
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
BordersAndZonesCollection.
FindObject
¶ Finds the
NXOpen.Drawings.BordersAndZones
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Drawing sheet name Returns: Borders and zones object Return type: NXOpen.Drawings.BordersAndZones
New in version NX8.0.0.
License requirements: None.