BordersAndZonesBuilderZoneMethod Enumeration¶
NXOpen.Drawings.BordersAndZonesBuilder.ZoneMethod is an alias for NXOpen.Drawings.BordersAndZonesBuilderZoneMethod
-
class
NXOpen.Drawings.
BordersAndZonesBuilderZoneMethod
¶ Bases:
object
the zone method
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.Method
instead.Enum Members
Enum Member Enum Member Description None NoneStandard StandardCustom -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-