BorderAndZoneStyleBuilder Class¶
-
class
NXOpen.Drawings.
BorderAndZoneStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Border and Zone Style Builder which manages all the style attributes related * to sheet borders, sheet margins and sheet zones.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BorderAndZoneStandard | Returns or sets the borders and zones standard |
SheetBorderSettingsStyle | Returns the drawing sheet border settings builder |
SheetMarginSettingsStyle | Returns the drawing sheet margin settings builder |
SheetZoneSettingsStyle | Returns the drawing sheet zone settings builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
InheritSettingsFromCustomerDefault | Inherit settings from customer default |
InheritSettingsFromPreferences | Inherit settings from preference |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BorderAndZoneStandard¶
-
BorderAndZoneStyleBuilder.
BorderAndZoneStandard
¶ Returns or sets the borders and zones standard
-------------------------------------
Getter Method
Signature
BorderAndZoneStandard()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BorderAndZoneStandard(borderAndZoneStandard)
Parameters: borderAndZoneStandard (int) – New in version NX10.0.0.
License requirements: None.
SheetBorderSettingsStyle¶
-
BorderAndZoneStyleBuilder.
SheetBorderSettingsStyle
¶ Returns the drawing sheet border settings builder
-------------------------------------
Getter Method
Signature
SheetBorderSettingsStyle()
Returns: Return type: NXOpen.Drawings.SheetBorderSettingsBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SheetMarginSettingsStyle¶
-
BorderAndZoneStyleBuilder.
SheetMarginSettingsStyle
¶ Returns the drawing sheet margin settings builder
-------------------------------------
Getter Method
Signature
SheetMarginSettingsStyle()
Returns: Return type: NXOpen.Drawings.SheetMarginSettingsBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SheetZoneSettingsStyle¶
-
BorderAndZoneStyleBuilder.
SheetZoneSettingsStyle
¶ Returns the drawing sheet zone settings builder
-------------------------------------
Getter Method
Signature
SheetZoneSettingsStyle()
Returns: Return type: NXOpen.Drawings.SheetZoneSettingsBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
InheritSettingsFromCustomerDefault¶
-
BorderAndZoneStyleBuilder.
InheritSettingsFromCustomerDefault
¶ Inherit settings from customer default
Signature
InheritSettingsFromCustomerDefault()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromPreferences¶
-
BorderAndZoneStyleBuilder.
InheritSettingsFromPreferences
¶ Inherit settings from preference
Signature
InheritSettingsFromPreferences()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
BorderAndZoneStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.