AutomationBookletBuilder Class¶
-
class
NXOpen.Drawings.
AutomationBookletBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.AutomationBookletBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
HiddenLineColorFontWidth | Returns the hidden line color font width |
Tag | Returns the Tag for this object. |
VisibleLineColorFontWidth | Returns the visible line color font width |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
VisibleLineColorFontWidth¶
-
AutomationBookletBuilder.
VisibleLineColorFontWidth
¶ Returns the visible line color font width
-------------------------------------
Getter Method
Signature
VisibleLineColorFontWidth()
Returns: Return type: NXOpen.LineColorFontWidthBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AutomationBookletBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.