DisplayManagerShowHideScope Enumeration¶
NXOpen.DisplayManager.ShowHideScope is an alias for NXOpen.DisplayManagerShowHideScope
-
class
NXOpen.
DisplayManagerShowHideScope
¶ Bases:
object
Controls the scope for the show hide operation.
See
ShowByType
andHideByType
Enum Members
Enum Member Enum Member Description AnyInAssembly Show and hide objects from the entire displayed partWorkPartAndOccurrence Show and hide objects only from the work part and its children-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-