StudioImageCaptureBuilder Class¶
-
class
NXOpen.Display.
StudioImageCaptureBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.StudioImageCaptureBuilder
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateStudioImageCaptureBuilder
Default values.
Property Value AASamplesEnum Sam0X DpiEnum Dpi72 DrawingSizeEnum Isoa4 OrientEnum Landscape UnitsEnum Pixels New in version NX6.0.4.
Properties¶
Property | Description |
---|---|
AASamplesEnum | Returns or sets the antialiasing samples enum |
DpiEnum | Returns or sets the dpi enum |
DrawingSizeEnum | Returns or sets the drawing size enum |
NativeFileBrowser | Returns or sets the native file browser for image type to produce |
OrientEnum | Returns or sets the orient enum |
Tag | Returns the Tag for this object. |
UnitsEnum | Returns or sets the units enum |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetImageDimensionsDouble | Gets the double image dimensions, height and width @return array of 2 doubles |
GetImageDimensionsInteger | Gets the integer image dimensions, height and width @return array of 2 integers |
GetObject | Returns the object currently being edited by this builder. |
SetImageDimensionsDouble | Sets the double image dimensions, height and width |
SetImageDimensionsInteger | Sets the integer image dimensions, height and width |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StudioImageCaptureBuilderAASamplesEnumType Enumeration | Provide the following anti-aliasing sample size for off screen image capture |
StudioImageCaptureBuilderDPIEnumType Enumeration | Provide the following screen capture resolutions in dots per inch |
StudioImageCaptureBuilderDrawingSizeEnumType Enumeration | Provide the following standard Drawing sizes |
StudioImageCaptureBuilderOrientEnumType Enumeration | Provide the following options to image orientation |
StudioImageCaptureBuilderUnitsEnumType Enumeration | Provide the following resolution unit options to screen capture |
Property Detail¶
AASamplesEnum¶
-
StudioImageCaptureBuilder.
AASamplesEnum
¶ Returns or sets the antialiasing samples enum
-------------------------------------
Getter Method
Signature
AASamplesEnum()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilderAASamplesEnumType
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
AASamplesEnum(aASamplesEnum)
Parameters: aASamplesEnum ( NXOpen.Display.StudioImageCaptureBuilderAASamplesEnumType
) –New in version NX6.0.4.
License requirements: None.
DpiEnum¶
-
StudioImageCaptureBuilder.
DpiEnum
¶ Returns or sets the dpi enum
-------------------------------------
Getter Method
Signature
DpiEnum()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilderDPIEnumType
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
DpiEnum(dpiEnum)
Parameters: dpiEnum ( NXOpen.Display.StudioImageCaptureBuilderDPIEnumType
) –New in version NX6.0.4.
License requirements: None.
DrawingSizeEnum¶
-
StudioImageCaptureBuilder.
DrawingSizeEnum
¶ Returns or sets the drawing size enum
-------------------------------------
Getter Method
Signature
DrawingSizeEnum()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilderDrawingSizeEnumType
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingSizeEnum(drawingSizeEnum)
Parameters: drawingSizeEnum ( NXOpen.Display.StudioImageCaptureBuilderDrawingSizeEnumType
) –New in version NX6.0.4.
License requirements: None.
NativeFileBrowser¶
-
StudioImageCaptureBuilder.
NativeFileBrowser
¶ Returns or sets the native file browser for image type to produce
-------------------------------------
Getter Method
Signature
NativeFileBrowser()
Returns: Return type: str New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
NativeFileBrowser(filename)
Parameters: filename (str) – New in version NX6.0.4.
License requirements: None.
OrientEnum¶
-
StudioImageCaptureBuilder.
OrientEnum
¶ Returns or sets the orient enum
-------------------------------------
Getter Method
Signature
OrientEnum()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilderOrientEnumType
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientEnum(orientEnum)
Parameters: orientEnum ( NXOpen.Display.StudioImageCaptureBuilderOrientEnumType
) –New in version NX6.0.4.
License requirements: None.
UnitsEnum¶
-
StudioImageCaptureBuilder.
UnitsEnum
¶ Returns or sets the units enum
-------------------------------------
Getter Method
Signature
UnitsEnum()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilderUnitsEnumType
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnitsEnum(unitsEnum)
Parameters: unitsEnum ( NXOpen.Display.StudioImageCaptureBuilderUnitsEnumType
) –New in version NX6.0.4.
License requirements: None.
Method Detail¶
GetImageDimensionsDouble¶
-
StudioImageCaptureBuilder.
GetImageDimensionsDouble
¶ Gets the double image dimensions, height and width
Signature
GetImageDimensionsDouble()
Returns: array of 2 doubles Return type: list of float New in version NX6.0.4.
License requirements: None.
GetImageDimensionsInteger¶
-
StudioImageCaptureBuilder.
GetImageDimensionsInteger
¶ Gets the integer image dimensions, height and width
Signature
GetImageDimensionsInteger()
Returns: array of 2 integers Return type: list of int New in version NX6.0.4.
License requirements: None.
SetImageDimensionsDouble¶
-
StudioImageCaptureBuilder.
SetImageDimensionsDouble
¶ Sets the double image dimensions, height and width
Signature
SetImageDimensionsDouble(imageDimensionsDouble)
Parameters: imageDimensionsDouble (list of float) – array of 2 doubles New in version NX6.0.4.
License requirements: None.
SetImageDimensionsInteger¶
-
StudioImageCaptureBuilder.
SetImageDimensionsInteger
¶ Sets the integer image dimensions, height and width
Signature
SetImageDimensionsInteger(imageDimensionsInteger)
Parameters: imageDimensionsInteger (list of int) – array of 2 integers New in version NX6.0.4.
License requirements: None.
Validate¶
-
StudioImageCaptureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.