LightBuilder Class¶
-
class
NXOpen.Display.
LightBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.LightBuilder
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateLightBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ConeAngle | Returns or sets the cone angle - only applicable to spot light types |
DestinationPosition | Returns or sets the destination position - only applicable to spot light types |
Intensity | Returns or sets the brightness intensity for a given light |
LightShadowType | Returns or sets the light shadow type - not applicable to ambient or eye light types |
LightType | Returns or sets the light type for a particular light |
SourcePosition | Returns or sets the source position - only applicable to spot and point light types |
Tag | Returns the Tag for this object. |
UseWithAdvancedStudioImageBasedLighting | Returns or sets the flag to indicate whether the given light is to be used with image based lighting in the advanced studio display. |
UseWithIbl | Returns or sets the use_with_ibl flag for a given light |
UseWithRayTracedImageBasedLighting | Returns or sets the flag to indicate whether the given light is to be used with image based lighting in ray traced rendering. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LightBuilderLightMode Enumeration | light_mode |
LightBuilderShadowType Enumeration | shadow types |
Property Detail¶
ConeAngle¶
-
LightBuilder.
ConeAngle
¶ Returns or sets the cone angle - only applicable to spot light types
-------------------------------------
Getter Method
Signature
ConeAngle()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConeAngle(coneAngle)
Parameters: coneAngle (float) – New in version NX5.0.0.
License requirements: None.
DestinationPosition¶
-
LightBuilder.
DestinationPosition
¶ Returns or sets the destination position - only applicable to spot light types
-------------------------------------
Getter Method
Signature
DestinationPosition()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationPosition(destinationPosition)
Parameters: destinationPosition ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
Intensity¶
-
LightBuilder.
Intensity
¶ Returns or sets the brightness intensity for a given light
-------------------------------------
Getter Method
Signature
Intensity()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Intensity(intensity)
Parameters: intensity (float) – New in version NX5.0.0.
License requirements: None.
LightShadowType¶
-
LightBuilder.
LightShadowType
¶ Returns or sets the light shadow type - not applicable to ambient or eye light types
-------------------------------------
Getter Method
Signature
LightShadowType()
Returns: Return type: NXOpen.Display.LightBuilderShadowType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightShadowType(lightShadowType)
Parameters: lightShadowType ( NXOpen.Display.LightBuilderShadowType
) –New in version NX5.0.0.
License requirements: None.
LightType¶
-
LightBuilder.
LightType
¶ Returns or sets the light type for a particular light
-------------------------------------
Getter Method
Signature
LightType()
Returns: Return type: NXOpen.LightType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightType(lightType)
Parameters: lightType ( NXOpen.LightType
) –New in version NX5.0.0.
License requirements: None.
SourcePosition¶
-
LightBuilder.
SourcePosition
¶ Returns or sets the source position - only applicable to spot and point light types
-------------------------------------
Getter Method
Signature
SourcePosition()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourcePosition(sourcePosition)
Parameters: sourcePosition ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
UseWithAdvancedStudioImageBasedLighting¶
-
LightBuilder.
UseWithAdvancedStudioImageBasedLighting
¶ Returns or sets the flag to indicate whether the given light is to be used with image based lighting in the advanced studio display.
-------------------------------------
Getter Method
Signature
UseWithAdvancedStudioImageBasedLighting()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseWithAdvancedStudioImageBasedLighting(useWithAdvancedStudioIBl)
Parameters: useWithAdvancedStudioIBl (bool) – New in version NX10.0.0.
License requirements: None.
UseWithIbl¶
-
LightBuilder.
UseWithIbl
¶ Returns or sets the use_with_ibl flag for a given light
-------------------------------------
Getter Method
Signature
UseWithIbl()
Returns: Return type: bool New in version NX5.0.0.
Deprecated since version NX10.0.0: This funcationality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseWithIbl(useWithIBL)
Parameters: useWithIBL (bool) – New in version NX5.0.0.
Deprecated since version NX10.0.0: This funcationality is no longer supported.
License requirements: None.
UseWithRayTracedImageBasedLighting¶
-
LightBuilder.
UseWithRayTracedImageBasedLighting
¶ Returns or sets the flag to indicate whether the given light is to be used with image based lighting in ray traced rendering.
-------------------------------------
Getter Method
Signature
UseWithRayTracedImageBasedLighting()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseWithRayTracedImageBasedLighting(useWithRayTracedIBL)
Parameters: useWithRayTracedIBL (bool) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LightBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.