LayerSettingsBuilder Class¶
-
class
NXOpen.Display.
LayerSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a builder for object layer settings.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Layer | Returns or sets the layer. |
LayerOption | Returns or sets the layer option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
IsValidLayerOption | Determines if the layer option is supported. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LayerSettingsBuilderLayerOptionType Enumeration | Specifies the layer options. |
Property Detail¶
Layer¶
-
LayerSettingsBuilder.
Layer
¶ Returns or sets the layer.
Used when the layer option is set to
Display.LayerSettingsBuilderLayerOptionType.UserDefined
. SeeNXOpen.Layer.Constants
for valid layer values.-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX9.0.0.
License requirements: None.
LayerOption¶
-
LayerSettingsBuilder.
LayerOption
¶ Returns or sets the layer option.
Note that all layer options may not be supported by the builder. Refer
Display.LayerSettingsBuilder.IsValidLayerOption
to determine supported options.-------------------------------------
Getter Method
Signature
LayerOption()
Returns: Return type: NXOpen.Display.LayerSettingsBuilderLayerOptionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption(layerOption)
Parameters: layerOption ( NXOpen.Display.LayerSettingsBuilderLayerOptionType
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
IsValidLayerOption¶
-
LayerSettingsBuilder.
IsValidLayerOption
¶ Determines if the layer option is supported.
The parent builder determines the validity of the layer options. For example, following layer options are not relevant when the layer is not being derived from another displayable object.
Display.LayerSettingsBuilderLayerOptionType.Maintain
Display.LayerSettingsBuilderLayerOptionType.Original
Signature
IsValidLayerOption(layerOption)
Parameters: layerOption ( NXOpen.Display.LayerSettingsBuilderLayerOptionType
) –Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
Validate¶
-
LayerSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.