ImageBaseBuilder Class¶
-
class
NXOpen.Display.
ImageBaseBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.ImageBaseBuilder
.Serves as the base class for all
NXOpen.Display.ImageBase
builders.NXOpen.Display.ImageBase
base class provides definition, orientation, sizing, and display setting controls for image based objects.This is an abstract class, and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BasePointChoice | Returns or sets the image reference base point choice. |
ColorMode | Returns or sets the color mode to display the image. |
Height |
|
ImageFile | Returns or sets the image file |
ImageReferencePoint1 |
|
ImageReferencePoint2 |
|
ImageReferencePoint3 |
|
InsertionPointOption | Returns or sets the image insertion point type |
LockAspectRatio | Returns or sets the lock aspect ratio |
ModelReferencePoint1 |
|
ModelReferencePoint2 |
|
ModelReferencePoint3 |
|
OverallTranslucency | Returns or sets the overall translucency. |
PixelColorTolerance | Returns or sets the transparency pixel color tolerance. |
ReferenceDirectionOption | Returns or sets the image alignment reference direction type. |
RotateAngleOfReferenceVector | Returns the current rotation angle of image from aligned reference direction |
SizeOption | Returns or sets the size option |
Tag | Returns the Tag for this object. |
TransparencyColorOption | Returns or sets the transparency color option |
UserBasePoint |
|
UserInsertionPoint | Returns or sets the user defined insertion point |
UserReferenceDirection | Returns or sets the user defined reference direction vector. |
Width |
|
Methods¶
Method | Description |
---|---|
AlignImageToReferenceDirection | Align Image to Reference Direction |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipHorizontal | Flips the image horizontally. |
FlipVertical | Flips the image vertically. |
GetBackgroundColor | Gets the background color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.ColorMode is set to NXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale . |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerPoints | Get the image corner points. |
GetForegroundColor | Gets the foreground color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.ColorMode is set to NXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale . |
GetImagesInPart | Provide a list of names of the NXOpen.Display.ImageData objects saved in current part file. |
GetObject | Returns the object currently being edited by this builder. |
GetTransparentPixelColor | Gets the transparency color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.TransparencyColorOption is set to NXOpen.Display.ImageBaseBuilderTransparencyColorFrom.PixelColor . |
OrientViewToImage | Orients and fits the work view’s view direction along the reverse normal direction of the image |
ResetImageSize | Resets the image to its original size. |
RotateLeft | Rotates the image 90 degrees counter-clockwise. |
RotateRight | Rotates the image 90 degrees clockwise. |
SetBackgroundColor | Sets the background color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.ColorMode is set to NXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale . |
SetCornerPoints | Set the image corner points. |
SetForegroundColor | Sets the foreground color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.ColorMode is set to NXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale . |
SetImageFromPart | Set a NXOpen.Display.ImageData object currently stored in the part as the image used by the builder. |
SetTransparentPixelColor | Sets the transparency color (RGB value) of the image. Only valid when NXOpen.Display.ImageBaseBuilder.TransparencyColorOption is set to NXOpen.Display.ImageBaseBuilderTransparencyColorFrom.PixelColor . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ImageBaseBuilderBasePointChoices Enumeration | Specifies image reference base point choice. |
ImageBaseBuilderImageColorModes Enumeration | Describes image color modes. |
ImageBaseBuilderInsertionPoint Enumeration | Describes insertion point type. |
ImageBaseBuilderReferenceDirection Enumeration | Specifies image alignment reference direction type. |
ImageBaseBuilderSizeOptions Enumeration | Describes size options. |
ImageBaseBuilderTransparencyColorFrom Enumeration | Transparency Color From |
Property Detail¶
BasePointChoice¶
-
ImageBaseBuilder.
BasePointChoice
¶ Returns or sets the image reference base point choice.
If you choose
NXOpen.Display.ImageBaseBuilderBasePointChoices.UserDefined
, useNXOpen.Display.ImageBaseBuilder.UserBasePoint
to set a point as the User-Defined point.-------------------------------------
Getter Method
Signature
BasePointChoice()
Returns: Return type: NXOpen.Display.ImageBaseBuilderBasePointChoices
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointChoice(basePoint)
Parameters: basePoint ( NXOpen.Display.ImageBaseBuilderBasePointChoices
) –New in version NX9.0.0.
License requirements: None.
ColorMode¶
-
ImageBaseBuilder.
ColorMode
¶ Returns or sets the color mode to display the image.
-------------------------------------
Getter Method
Signature
ColorMode()
Returns: Return type: NXOpen.Display.ImageBaseBuilderImageColorModes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorMode(colorMode)
Parameters: colorMode ( NXOpen.Display.ImageBaseBuilderImageColorModes
) –New in version NX9.0.0.
License requirements: None.
Height¶
-
ImageBaseBuilder.
Height
¶ Returns the height of the image as an
NXOpen.Expression
. The returnedNXOpen.Expression
is **not</b> associative to this object.When
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.UserDefined
, set the size of the image usingNXOpen.Display.ImageBaseBuilder.SetCornerPoints
.-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ImageFile¶
-
ImageBaseBuilder.
ImageFile
¶ Returns or sets the image file
-------------------------------------
Getter Method
Signature
ImageFile()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageFile(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: None.
ImageReferencePoint1¶
-
ImageBaseBuilder.
ImageReferencePoint1
¶ Returns or sets the image reference point1. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ImageReferencePoint1()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageReferencePoint1(imageReferencePoint1)
Parameters: imageReferencePoint1 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
ImageReferencePoint2¶
-
ImageBaseBuilder.
ImageReferencePoint2
¶ Returns or sets the image reference point2. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ImageReferencePoint2()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageReferencePoint2(imageReferencePoint2)
Parameters: imageReferencePoint2 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
ImageReferencePoint3¶
-
ImageBaseBuilder.
ImageReferencePoint3
¶ Returns or sets the image reference point3. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
andNXOpen.Display.ImageBaseBuilder.LockAspectRatio
is False.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ImageReferencePoint3()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageReferencePoint3(imageReferencePoint3)
Parameters: imageReferencePoint3 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
InsertionPointOption¶
-
ImageBaseBuilder.
InsertionPointOption
¶ Returns or sets the image insertion point type
-------------------------------------
Getter Method
Signature
InsertionPointOption()
Returns: Return type: NXOpen.Display.ImageBaseBuilderInsertionPoint
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertionPointOption(insertPoint)
Parameters: insertPoint ( NXOpen.Display.ImageBaseBuilderInsertionPoint
) –New in version NX9.0.0.
License requirements: None.
LockAspectRatio¶
-
ImageBaseBuilder.
LockAspectRatio
¶ Returns or sets the lock aspect ratio
-------------------------------------
Getter Method
Signature
LockAspectRatio()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockAspectRatio(lockAspectRatio)
Parameters: lockAspectRatio (bool) – New in version NX9.0.0.
License requirements: None.
ModelReferencePoint1¶
-
ImageBaseBuilder.
ModelReferencePoint1
¶ Returns or sets the model reference point1. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ModelReferencePoint1()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelReferencePoint1(modelReferencePoint1)
Parameters: modelReferencePoint1 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
ModelReferencePoint2¶
-
ImageBaseBuilder.
ModelReferencePoint2
¶ Returns or sets the model reference point2. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ModelReferencePoint2()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelReferencePoint2(modelReferencePoint2)
Parameters: modelReferencePoint2 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
ModelReferencePoint3¶
-
ImageBaseBuilder.
ModelReferencePoint3
¶ Returns or sets the model reference point3. Only valid when
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.ReferenceScaling
andNXOpen.Display.ImageBaseBuilder.LockAspectRatio
is False.Reference Scaling provides sizing the image by defining image reference points and matching them with corresponding model reference points.
-------------------------------------
Getter Method
Signature
ModelReferencePoint3()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelReferencePoint3(modelReferencePoint3)
Parameters: modelReferencePoint3 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
OverallTranslucency¶
-
ImageBaseBuilder.
OverallTranslucency
¶ Returns or sets the overall translucency.
The range of this value is 0 to 100.
-------------------------------------
Getter Method
Signature
OverallTranslucency()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverallTranslucency(overallTranslucency)
Parameters: overallTranslucency (int) – New in version NX9.0.0.
License requirements: None.
PixelColorTolerance¶
-
ImageBaseBuilder.
PixelColorTolerance
¶ Returns or sets the transparency pixel color tolerance.
The range of this value is 0 to 255.
-------------------------------------
Getter Method
Signature
PixelColorTolerance()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PixelColorTolerance(colorTolerence)
Parameters: colorTolerence (int) – New in version NX9.0.0.
License requirements: None.
ReferenceDirectionOption¶
-
ImageBaseBuilder.
ReferenceDirectionOption
¶ Returns or sets the image alignment reference direction type.
NXOpen.Display.ImageBaseBuilderReferenceDirection.Horizontal
means rotate the image to align its horizontal direction with the user-specified reference direction (if defined).-------------------------------------
Getter Method
Signature
ReferenceDirectionOption()
Returns: Return type: NXOpen.Display.ImageBaseBuilderReferenceDirection
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDirectionOption(referenceDirection)
Parameters: referenceDirection ( NXOpen.Display.ImageBaseBuilderReferenceDirection
) –New in version NX9.0.0.
License requirements: None.
RotateAngleOfReferenceVector¶
-
ImageBaseBuilder.
RotateAngleOfReferenceVector
¶ Returns the current rotation angle of image from aligned reference direction
-------------------------------------
Getter Method
Signature
RotateAngleOfReferenceVector()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SizeOption¶
-
ImageBaseBuilder.
SizeOption
¶ Returns or sets the size option
-------------------------------------
Getter Method
Signature
SizeOption()
Returns: Return type: NXOpen.Display.ImageBaseBuilderSizeOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizeOption(sizeOption)
Parameters: sizeOption ( NXOpen.Display.ImageBaseBuilderSizeOptions
) –New in version NX9.0.0.
License requirements: None.
TransparencyColorOption¶
-
ImageBaseBuilder.
TransparencyColorOption
¶ Returns or sets the transparency color option
-------------------------------------
Getter Method
Signature
TransparencyColorOption()
Returns: Return type: NXOpen.Display.ImageBaseBuilderTransparencyColorFrom
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransparencyColorOption(transparencyColorOption)
Parameters: transparencyColorOption ( NXOpen.Display.ImageBaseBuilderTransparencyColorFrom
) –New in version NX9.0.0.
License requirements: None.
UserBasePoint¶
-
ImageBaseBuilder.
UserBasePoint
¶ Returns or sets the user defined base point. Only valid when
NXOpen.Display.ImageBaseBuilder.BasePointChoice
is set toNXOpen.Display.ImageBaseBuilderBasePointChoices.UserDefined
.-------------------------------------
Getter Method
Signature
UserBasePoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserBasePoint(basePoint)
Parameters: basePoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
UserInsertionPoint¶
-
ImageBaseBuilder.
UserInsertionPoint
¶ Returns or sets the user defined insertion point
-------------------------------------
Getter Method
Signature
UserInsertionPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserInsertionPoint(insertPoint)
Parameters: insertPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
UserReferenceDirection¶
-
ImageBaseBuilder.
UserReferenceDirection
¶ Returns or sets the user defined reference direction vector.
A direction normal to the plane of the image is invalid.
-------------------------------------
Getter Method
Signature
UserReferenceDirection()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserReferenceDirection(userDirection)
Parameters: userDirection ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: None.
Width¶
-
ImageBaseBuilder.
Width
¶ Returns the width of the image as an
NXOpen.Expression
. The returnedNXOpen.Expression
is **not</b> associative to this object.When
NXOpen.Display.ImageBaseBuilder.SizeOption
is set toNXOpen.Display.ImageBaseBuilderSizeOptions.UserDefined
, set the size of the image usingNXOpen.Display.ImageBaseBuilder.SetCornerPoints
.-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
AlignImageToReferenceDirection¶
-
ImageBaseBuilder.
AlignImageToReferenceDirection
¶ Align Image to Reference Direction
Signature
AlignImageToReferenceDirection()
New in version NX9.0.0.
License requirements: None.
FlipHorizontal¶
-
ImageBaseBuilder.
FlipHorizontal
¶ Flips the image horizontally.
Signature
FlipHorizontal()
New in version NX9.0.0.
License requirements: None.
FlipVertical¶
-
ImageBaseBuilder.
FlipVertical
¶ Flips the image vertically.
Signature
FlipVertical()
New in version NX9.0.0.
License requirements: None.
GetBackgroundColor¶
-
ImageBaseBuilder.
GetBackgroundColor
¶ Gets the background color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.ColorMode
is set toNXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale
.The length of the output array will always be 3. Each color value of the double array is in the range 0.0 to 1.0.
Signature
GetBackgroundColor()
Returns: RGB color array Return type: list of float New in version NX9.0.0.
License requirements: None.
GetCornerPoints¶
-
ImageBaseBuilder.
GetCornerPoints
¶ Get the image corner points.
The points define a rectangular region and are ordered counter-clockwise.
Signature
GetCornerPoints()
Returns: a tuple Return type: A tuple consisting of (point1, point2, point3, point4). point1 is a NXOpen.Point3d
. first corner point of image point2 is aNXOpen.Point3d
. second corner point of image point3 is aNXOpen.Point3d
. third corner point of image point4 is aNXOpen.Point3d
. fourth corner point of imageNew in version NX9.0.0.
License requirements: None.
GetForegroundColor¶
-
ImageBaseBuilder.
GetForegroundColor
¶ Gets the foreground color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.ColorMode
is set toNXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale
.The length of the output array will always be 3. Each color value of the double array is in the range 0.0 to 1.0.
Signature
GetForegroundColor()
Returns: RGB color array Return type: list of float New in version NX9.0.0.
License requirements: None.
GetImagesInPart¶
-
ImageBaseBuilder.
GetImagesInPart
¶ Provide a list of names of the
NXOpen.Display.ImageData
objects saved in current part file.Signature
GetImagesInPart()
Returns: Array of NXOpen.Display.ImageData
namesReturn type: list of str New in version NX9.0.0.
License requirements: None.
GetTransparentPixelColor¶
-
ImageBaseBuilder.
GetTransparentPixelColor
¶ Gets the transparency color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.TransparencyColorOption
is set toNXOpen.Display.ImageBaseBuilderTransparencyColorFrom.PixelColor
.The length of the output array will always be 3. Each color value of the double array is in the range 0.0 to 1.0.
Signature
GetTransparentPixelColor()
Returns: RGB color array Return type: list of float New in version NX9.0.0.
License requirements: None.
OrientViewToImage¶
-
ImageBaseBuilder.
OrientViewToImage
¶ Orients and fits the work view’s view direction along the reverse normal direction of the image
Signature
OrientViewToImage()
New in version NX9.0.0.
License requirements: None.
ResetImageSize¶
-
ImageBaseBuilder.
ResetImageSize
¶ Resets the image to its original size.
Signature
ResetImageSize()
New in version NX9.0.0.
License requirements: None.
RotateLeft¶
-
ImageBaseBuilder.
RotateLeft
¶ Rotates the image 90 degrees counter-clockwise.
Signature
RotateLeft()
New in version NX9.0.0.
License requirements: None.
RotateRight¶
-
ImageBaseBuilder.
RotateRight
¶ Rotates the image 90 degrees clockwise.
Signature
RotateRight()
New in version NX9.0.0.
License requirements: None.
SetBackgroundColor¶
-
ImageBaseBuilder.
SetBackgroundColor
¶ Sets the background color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.ColorMode
is set toNXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale
.The length of the input array should always be 3. Each color value of the double array must be in the range 0.0 to 1.0.
Signature
SetBackgroundColor(backgroundColor)
Parameters: backgroundColor (list of float) – RGB color array New in version NX9.0.0.
License requirements: None.
SetCornerPoints¶
-
ImageBaseBuilder.
SetCornerPoints
¶ Set the image corner points.
The points must define a rectangular region and be ordered counter-clockwise.
Signature
SetCornerPoints(point1, point2, point3, point4)
Parameters: - point1 (
NXOpen.Point3d
) – first corner point of image - point2 (
NXOpen.Point3d
) – second corner point of image - point3 (
NXOpen.Point3d
) – third corner point of image - point4 (
NXOpen.Point3d
) – fourth corner point of image
New in version NX9.0.0.
License requirements: None.
- point1 (
SetForegroundColor¶
-
ImageBaseBuilder.
SetForegroundColor
¶ Sets the foreground color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.ColorMode
is set toNXOpen.Display.ImageBaseBuilderImageColorModes.Greyscale
.The length of the input array should always be 3. Each color value of the double array must be in the range 0.0 to 1.0.
Signature
SetForegroundColor(foregroundColor)
Parameters: foregroundColor (list of float) – RGB color array New in version NX9.0.0.
License requirements: None.
SetImageFromPart¶
-
ImageBaseBuilder.
SetImageFromPart
¶ Set a
NXOpen.Display.ImageData
object currently stored in the part as the image used by the builder.Signature
SetImageFromPart(imageName)
Parameters: imageName (str) – Name of NXOpen.Display.ImageData
objectNew in version NX9.0.0.
License requirements: None.
SetTransparentPixelColor¶
-
ImageBaseBuilder.
SetTransparentPixelColor
¶ Sets the transparency color (RGB value) of the image. Only valid when
NXOpen.Display.ImageBaseBuilder.TransparencyColorOption
is set toNXOpen.Display.ImageBaseBuilderTransparencyColorFrom.PixelColor
.The length of the input array should always be 3. Each color value of the double array must be in the range 0.0 to 1.0.
Signature
SetTransparentPixelColor(transparencyColor)
Parameters: transparencyColor (list of float) – RGB color array New in version NX9.0.0.
License requirements: None.
Validate¶
-
ImageBaseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.