DecalBuilder Class¶
-
class
NXOpen.Display.
DecalBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.DecalBuilder
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AnchorType | Returns or sets the anchor type |
AspectRatio | Returns or sets the decal image aspect ratio |
DecalName | Returns or sets the decal name |
DecalReflectivity | Returns or sets the decal reflectivity |
EnableEngraving | Returns or sets the engraving enable toggle |
EngravingAmplitude | Returns or sets the decal engraving amplitude |
EngravingSoftness | Returns or sets the engraving softness |
HeightScale | Returns or sets the decal height scale |
IlluminationType | Returns or sets the illumination type |
Image | Returns or sets the image builder |
ImageFilename | Returns or sets the decal image file name |
ImageSizeType | Returns or sets the image size type |
NormalVector | Returns or sets the decal normal vector |
NormalVectorValue | Returns or sets the decal normal vector value |
Object | Returns the object(face, body and facetted body) to apply the decal to |
Origin | Returns or sets the origin |
OriginPosition | Returns or sets the origin_pos |
Rotation | Returns or sets the decal rotation |
Scale | Returns or sets the decal scale |
ScalingType | Returns or sets the scaling type |
StencilPreview | Returns or sets the stencil preview toggle |
Tag | Returns the Tag for this object. |
TransparencyTolerance | Returns or sets the transparency tolerance |
UpVector | Returns or sets the decal up vector |
UpVectorValue | Returns or sets the decal up vector value |
WidthScale | Returns or sets the decal width scale |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetImagesInPart | Provide a list of names of the NXOpen.Display.ImageData objects saved in current part file. |
GetTransparencyColor | Returns the transparency color @return |
SetImageFromPart | Set a NXOpen.Display.ImageData object currently stored in the part as the image used by the builder. |
SetTransparencyColor | Sets the transparency color |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DecalBuilderAnchor Enumeration | image anchor |
DecalBuilderDecalIllumination Enumeration | decal illumination type |
DecalBuilderImageSize Enumeration | image size type |
DecalBuilderScaling Enumeration | decal scaling type |
Property Detail¶
AnchorType¶
-
DecalBuilder.
AnchorType
¶ Returns or sets the anchor type
-------------------------------------
Getter Method
Signature
AnchorType()
Returns: Return type: NXOpen.Display.DecalBuilderAnchor
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorType(anchorType)
Parameters: anchorType ( NXOpen.Display.DecalBuilderAnchor
) –New in version NX6.0.0.
License requirements: None.
AspectRatio¶
-
DecalBuilder.
AspectRatio
¶ Returns or sets the decal image aspect ratio
-------------------------------------
Getter Method
Signature
AspectRatio()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AspectRatio(aspectRatio)
Parameters: aspectRatio (float) – New in version NX6.0.0.
License requirements: None.
DecalName¶
-
DecalBuilder.
DecalName
¶ Returns or sets the decal name
-------------------------------------
Getter Method
Signature
DecalName()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DecalName(decalName)
Parameters: decalName (str) – New in version NX6.0.0.
License requirements: None.
DecalReflectivity¶
-
DecalBuilder.
DecalReflectivity
¶ Returns or sets the decal reflectivity
-------------------------------------
Getter Method
Signature
DecalReflectivity()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DecalReflectivity(decalReflectivity)
Parameters: decalReflectivity (float) – New in version NX6.0.0.
License requirements: None.
EnableEngraving¶
-
DecalBuilder.
EnableEngraving
¶ Returns or sets the engraving enable toggle
-------------------------------------
Getter Method
Signature
EnableEngraving()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableEngraving(enableEngraving)
Parameters: enableEngraving (bool) – New in version NX6.0.0.
License requirements: None.
EngravingAmplitude¶
-
DecalBuilder.
EngravingAmplitude
¶ Returns or sets the decal engraving amplitude
-------------------------------------
Getter Method
Signature
EngravingAmplitude()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EngravingAmplitude(engravingAmplitude)
Parameters: engravingAmplitude (float) – New in version NX6.0.0.
License requirements: None.
EngravingSoftness¶
-
DecalBuilder.
EngravingSoftness
¶ Returns or sets the engraving softness
-------------------------------------
Getter Method
Signature
EngravingSoftness()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EngravingSoftness(engravingSoftness)
Parameters: engravingSoftness (float) – New in version NX6.0.0.
License requirements: None.
HeightScale¶
-
DecalBuilder.
HeightScale
¶ Returns or sets the decal height scale
-------------------------------------
Getter Method
Signature
HeightScale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeightScale(heightScale)
Parameters: heightScale (float) – New in version NX6.0.0.
License requirements: None.
IlluminationType¶
-
DecalBuilder.
IlluminationType
¶ Returns or sets the illumination type
-------------------------------------
Getter Method
Signature
IlluminationType()
Returns: Return type: NXOpen.Display.DecalBuilderDecalIllumination
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IlluminationType(illuminationType)
Parameters: illuminationType ( NXOpen.Display.DecalBuilderDecalIllumination
) –New in version NX6.0.0.
License requirements: None.
Image¶
-
DecalBuilder.
Image
¶ Returns or sets the image builder
-------------------------------------
Getter Method
Signature
Image()
Returns: Return type: NXOpen.Display.Image
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Image(imageBuilder)
Parameters: imageBuilder ( NXOpen.Display.Image
) –New in version NX6.0.0.
License requirements: None.
ImageFilename¶
-
DecalBuilder.
ImageFilename
¶ Returns or sets the decal image file name
-------------------------------------
Getter Method
Signature
ImageFilename()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageFilename(imageFileName)
Parameters: imageFileName (str) – New in version NX6.0.0.
License requirements: None.
ImageSizeType¶
-
DecalBuilder.
ImageSizeType
¶ Returns or sets the image size type
-------------------------------------
Getter Method
Signature
ImageSizeType()
Returns: Return type: NXOpen.Display.DecalBuilderImageSize
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageSizeType(imageSizeType)
Parameters: imageSizeType ( NXOpen.Display.DecalBuilderImageSize
) –New in version NX6.0.0.
License requirements: None.
NormalVector¶
-
DecalBuilder.
NormalVector
¶ Returns or sets the decal normal vector
-------------------------------------
Getter Method
Signature
NormalVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVector(normalVector)
Parameters: normalVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: None.
NormalVectorValue¶
-
DecalBuilder.
NormalVectorValue
¶ Returns or sets the decal normal vector value
-------------------------------------
Getter Method
Signature
NormalVectorValue()
Returns: Return type: NXOpen.Vector3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorValue(normalVectorValue)
Parameters: normalVectorValue ( NXOpen.Vector3d
) –New in version NX6.0.0.
License requirements: None.
Object¶
-
DecalBuilder.
Object
¶ Returns the object(face, body and facetted body) to apply the decal to
-------------------------------------
Getter Method
Signature
Object()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
Origin¶
-
DecalBuilder.
Origin
¶ Returns or sets the origin
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin(origin)
Parameters: origin ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
OriginPosition¶
-
DecalBuilder.
OriginPosition
¶ Returns or sets the origin_pos
-------------------------------------
Getter Method
Signature
OriginPosition()
Returns: Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginPosition(originPosition)
Parameters: originPosition ( NXOpen.Point3d
) –New in version NX6.0.0.
License requirements: None.
Rotation¶
-
DecalBuilder.
Rotation
¶ Returns or sets the decal rotation
-------------------------------------
Getter Method
Signature
Rotation()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rotation(rotation)
Parameters: rotation (float) – New in version NX6.0.0.
License requirements: None.
Scale¶
-
DecalBuilder.
Scale
¶ Returns or sets the decal scale
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX6.0.0.
License requirements: None.
ScalingType¶
-
DecalBuilder.
ScalingType
¶ Returns or sets the scaling type
-------------------------------------
Getter Method
Signature
ScalingType()
Returns: Return type: NXOpen.Display.DecalBuilderScaling
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingType(scalingType)
Parameters: scalingType ( NXOpen.Display.DecalBuilderScaling
) –New in version NX6.0.0.
License requirements: None.
StencilPreview¶
-
DecalBuilder.
StencilPreview
¶ Returns or sets the stencil preview toggle
-------------------------------------
Getter Method
Signature
StencilPreview()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StencilPreview(stencilPreview)
Parameters: stencilPreview (bool) – New in version NX6.0.0.
License requirements: None.
TransparencyTolerance¶
-
DecalBuilder.
TransparencyTolerance
¶ Returns or sets the transparency tolerance
-------------------------------------
Getter Method
Signature
TransparencyTolerance()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransparencyTolerance(transparencyTolerance)
Parameters: transparencyTolerance (int) – New in version NX6.0.0.
License requirements: None.
UpVector¶
-
DecalBuilder.
UpVector
¶ Returns or sets the decal up vector
-------------------------------------
Getter Method
Signature
UpVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpVector(upVector)
Parameters: upVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: None.
UpVectorValue¶
-
DecalBuilder.
UpVectorValue
¶ Returns or sets the decal up vector value
-------------------------------------
Getter Method
Signature
UpVectorValue()
Returns: Return type: NXOpen.Vector3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpVectorValue(upVectorValue)
Parameters: upVectorValue ( NXOpen.Vector3d
) –New in version NX6.0.0.
License requirements: None.
WidthScale¶
-
DecalBuilder.
WidthScale
¶ Returns or sets the decal width scale
-------------------------------------
Getter Method
Signature
WidthScale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WidthScale(widthScale)
Parameters: widthScale (float) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetImagesInPart¶
-
DecalBuilder.
GetImagesInPart
¶ Provide a list of names of the
NXOpen.Display.ImageData
objects saved in current part file.Signature
GetImagesInPart()
Returns: Array of NXOpen.Display.ImageData
namesReturn type: list of str New in version NX10.0.0.
License requirements: None.
GetTransparencyColor¶
-
DecalBuilder.
GetTransparencyColor
¶ Returns the transparency color
Signature
GetTransparencyColor()
Returns: Return type: list of float New in version NX6.0.0.
License requirements: None.
SetImageFromPart¶
-
DecalBuilder.
SetImageFromPart
¶ Set a
NXOpen.Display.ImageData
object currently stored in the part as the image used by the builder.Signature
SetImageFromPart(imageName)
Parameters: imageName (str) – Name of NXOpen.Display.ImageData
objectNew in version NX10.0.0.
License requirements: None.
SetTransparencyColor¶
-
DecalBuilder.
SetTransparencyColor
¶ Sets the transparency color
Signature
SetTransparencyColor(transparencyColor)
Parameters: transparencyColor (list of float) – New in version NX6.0.0.
License requirements: None.
Validate¶
-
DecalBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.