CustomPopupMenu Class

class NXOpen.CustomPopupMenu

Bases: NXOpen.CustomPopupMenuItem

Represents Custom Popup Menu Item class

New in version NX6.0.4.

Methods

Method Description
AddMenu Adds and returns a menu to this menu @return menu
AddMenuItem Adds and returns a menu item to this menu @return menu item
AddMenuSeparator Adds a separator in the submenu
Dispose Frees the object from memory.
GetId Returns Id of the menu item.
GetName Returns name of the menu item.
SetDisabled Sets the menu disabled

Method Detail

AddMenu

CustomPopupMenu.AddMenu

Adds and returns a menu to this menu

Signature AddMenu(menuId, menuName)

Parameters:
  • menuId (int) – Id of the menu
  • menuName (str) – name of the menu NOTE: The full Unicode character set is not supported for this parameter.
Returns:

menu

Return type:

NXOpen.CustomPopupMenu

New in version NX6.0.4.

License requirements: None.

AddMenuItem

CustomPopupMenu.AddMenuItem

Adds and returns a menu item to this menu

Signature AddMenuItem(menuItemId, menuItemName)

Parameters:
  • menuItemId (int) – Id of the menu item
  • menuItemName (str) – name of the menu item NOTE: The full Unicode character set is not supported for this parameter.
Returns:

menu item

Return type:

NXOpen.CustomPopupMenuItem

New in version NX6.0.4.

License requirements: None.

AddMenuSeparator

CustomPopupMenu.AddMenuSeparator

Adds a separator in the submenu

Signature AddMenuSeparator()

New in version NX6.0.4.

License requirements: None.

Dispose

CustomPopupMenu.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.4.

License requirements: None.