CurveCollection Class¶
-
class
NXOpen.
CurveCollection
¶ Bases:
object
Represents a collection of
NXOpen.Curve
.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Curve
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateArc | Creates an NXOpen.Arc that passes through the three specified points. |
CreateEllipse | Creates an NXOpen.Ellipse . |
CreateExtractedCurve | Creates a NXOpen.Curve . |
CreateHyperbola | Creates a NXOpen.Hyperbola . |
CreateInfiniteLine | Creates a NXOpen.InfiniteLine that passes through the two specified points. |
CreateLine | Creates a NXOpen.Line . |
CreatePairedInfiniteLine | Creates a paired NXOpen.InfiniteLine that is paired to the specified line. |
CreateParabola | Creates a NXOpen.Parabola . |
CreateSmartCompositeCurve | Creates a NXOpen.Curve . |
CreateVirtualBlendCurve | Creates a NXOpen.Curve . |
CreateVirtualCenterlineCurve | Creates a NXOpen.Curve . |
Method Detail¶
CreateArc¶
-
CurveCollection.
CreateArc
¶ Overloaded method CreateArc
CreateArc(startPoint, pointOn, endPoint, alternateSolution)
CreateArc(startPoint, pointOn, endPoint, alternateSolution)
CreateArc(center, matrix, radius, startAngle, endAngle)
CreateArc(center, xDirection, yDirection, radius, startAngle, endAngle)
-------------------------------------
Creates an
NXOpen.Arc
that passes through the three specified points.Signature
CreateArc(startPoint, pointOn, endPoint, alternateSolution)
Parameters: - startPoint (
NXOpen.Point3d
) – Start point - pointOn (
NXOpen.Point3d
) – Point that the arc passes through. - endPoint (
NXOpen.Point3d
) – End point - alternateSolution (bool) – If true, the arc will be created using the alternate solution instead of the regular solution. The alternate solution for an arc is the portion of the full circle that is left out of the regular solution. For example, if the regular solution is an arc that goes from 0 to 45 degrees, the alternate solution will be an arc with the same center and origin but that goes from 45 degrees to 360.
Returns: a tuple
Return type: A tuple consisting of (arc, startAndEndGotFlipped). arc is a
NXOpen.Arc
. startAndEndGotFlipped is a bool. If true, the start point of the arc that is created is at the end point parameter to this method and the end point of the arc is at the start point parameter. In other words, suppose you execute arc = Curves.CreateArc(startPointParam, pointOnParam, endPointParam, false, flipped). If flipped is true, then arc.StartPoint equals endPointParam and arc.EndPoint equals startPointParam.New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates an
NXOpen.Arc
. The arc will be created in a plane which passes through center and whose normal is the Z axis of the orientation matrix. (matrix.Element.xx, matrix.Element.xy, matrix.Element.xz) is the X axis of the orientation matrix. (matrix.Element.yx, matrix.Element.yy, matrix.Element.yz) is the Y axis of the orientation matrix. The start and end angles are measured relative to the X and Y axis of this orientation matrix.Signature
CreateArc(center, matrix, radius, startAngle, endAngle)
Parameters: - center (
NXOpen.Point3d
) – Center of the arc - matrix (
NXOpen.NXMatrix
) – Orientation matrix for the arc. - radius (float) – Radius of the arc. Must be greater than zero.
- startAngle (float) – Start angle in radians
- endAngle (float) – End angle in radians
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates an
NXOpen.Arc
. The arc will be created through the origin and whose normal is Z axis. The start and end angles are measured relative to the X and Y axes.Signature
CreateArc(center, xDirection, yDirection, radius, startAngle, endAngle)
Parameters: - center (
NXOpen.Point3d
) – Center of the arc - xDirection (
NXOpen.Vector3d
) – X direction of the arc - yDirection (
NXOpen.Vector3d
) – Y direction of the arc - radius (float) – Radius of the arc. Must be greater than zero.
- startAngle (float) – Start angle in radians
- endAngle (float) – End angle in radians
Returns: Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateEllipse¶
-
CurveCollection.
CreateEllipse
¶ Overloaded method CreateEllipse
CreateEllipse(center, majorRadius, minorRadius, startAngle, endAngle, rotationAngle, matrix)
CreateEllipse(center, xDirection, yDirection, majorRadius, minorRadius, startAngle, endAngle)
-------------------------------------
Creates an
NXOpen.Ellipse
. The ellipse will be created in a plane which passes through center and whose normal is the Z axis of the orientation matrix. (matrix.Element.xx, matrix.Element.xy, matrix.Element.xz) is the X axis of the orientation matrix. (matrix.Element.yx, matrix.Element.yy, matrix.Element.yz) is the Y axis of the orientation matrix. The start, end, and rotation angles are measured relative to the X and Y axis of this orientation matrix.Signature
CreateEllipse(center, majorRadius, minorRadius, startAngle, endAngle, rotationAngle, matrix)
Parameters: - center (
NXOpen.Point3d
) – Center of ellipse - majorRadius (float) – Major radius
- minorRadius (float) – Minor radius
- startAngle (float) – Start angle in radians
- endAngle (float) – End angle in radians
- rotationAngle (float) – Rotation angle in radians
- matrix (
NXOpen.NXMatrix
) – Orientation matrix for the ellipse
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates an
NXOpen.Ellipse
. The ellipse will be created through the origin and whose normal is Z axis. The start and end angles are measured relative to the X and Y axes.Signature
CreateEllipse(center, xDirection, yDirection, majorRadius, minorRadius, startAngle, endAngle)
Parameters: - center (
NXOpen.Point3d
) – Center of the ellipse - xDirection (
NXOpen.Vector3d
) – X direction of the ellipse - yDirection (
NXOpen.Vector3d
) – Y direction of the ellipse - majorRadius (float) – Major radius of the ellipse. Must be greater than zero.
- minorRadius (float) – Minor radius of the ellipse. Must be greater than zero.
- startAngle (float) – Start angle in radians
- endAngle (float) – End angle in radians
Returns: Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateExtractedCurve¶
-
CurveCollection.
CreateExtractedCurve
¶ Creates a
NXOpen.Curve
.The extracted curve will be created for the input curve to extract.
Signature
CreateExtractedCurve(curveToExtract, type, subtype, xform, tolerance, updateOption)
Parameters: - curveToExtract (
NXOpen.ICurve
) – Curve or edge to be extracted - type (int) – Type
- subtype (int) – Sub-Type
- xform (
NXOpen.Xform
) – optional Xform - tolerance (float) – tolerance for computing the extract curve
- updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
- curveToExtract (
CreateHyperbola¶
-
CurveCollection.
CreateHyperbola
¶ Overloaded method CreateHyperbola
CreateHyperbola(center, semiTransverseLength, semiConjugateLength, minimumDY, maximumDY, rotationAngle, matrix)
CreateHyperbola(center, xDirection, yDirection, semiTransverseLength, semiConjugateLength, minimumDY, maximumDY)
-------------------------------------
Creates a
NXOpen.Hyperbola
. The hyperbola will be created in a plane which passes through center and whose normal is the Z axis of the orientation matrix. (matrix.Element.xx, matrix.Element.xy, matrix.Element.xz) is the X axis of the orientation matrix. (matrix.Element.yx, matrix.Element.yy, matrix.Element.yz) is the Y axis of the orientation matrix. The rotation angle is measured relative to the X and Y axis of this orientation matrix.Signature
CreateHyperbola(center, semiTransverseLength, semiConjugateLength, minimumDY, maximumDY, rotationAngle, matrix)
Parameters: - center (
NXOpen.Point3d
) – Center of hyperbola - semiTransverseLength (float) – Semi-transverse length
- semiConjugateLength (float) – Semi-conjugate length
- minimumDY (float) – Minimum DY width
- maximumDY (float) – Maximum DY width
- rotationAngle (float) – Rotation angle in radians
- matrix (
NXOpen.NXMatrix
) – Orientation matrix for the hyperbola
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Hyperbola
. The hyperbola will be created through the origin and whose normal is Z axis.Signature
CreateHyperbola(center, xDirection, yDirection, semiTransverseLength, semiConjugateLength, minimumDY, maximumDY)
Parameters: - center (
NXOpen.Point3d
) – Center of the hyperbola - xDirection (
NXOpen.Vector3d
) – X direction of the hyperbola - yDirection (
NXOpen.Vector3d
) – Y direction of the hyperbola - semiTransverseLength (float) – Semi-transverse length
- semiConjugateLength (float) – Semi-conjugate length
- minimumDY (float) – Minimum DY width
- maximumDY (float) – Maximum DY width
Returns: Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateInfiniteLine¶
-
CurveCollection.
CreateInfiniteLine
¶ Creates a
NXOpen.InfiniteLine
that passes through the two specified points.Signature
CreateInfiniteLine(startPoint, endPoint)
Parameters: - startPoint (
NXOpen.Point3d
) – Start point - endPoint (
NXOpen.Point3d
) – End point
Returns: Return type: New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
- startPoint (
CreateLine¶
-
CurveCollection.
CreateLine
¶ Overloaded method CreateLine
CreateLine(startPoint, endPoint)
CreateLine(startPoint, endPoint)
-------------------------------------
Creates a
NXOpen.Line
.Signature
CreateLine(startPoint, endPoint)
Parameters: - startPoint (
NXOpen.Point3d
) – Start point - endPoint (
NXOpen.Point3d
) – End point
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Line
joining given startNXOpen.Point
and EndNXOpen.Point
.Signature
CreateLine(startPoint, endPoint)
Parameters: - startPoint (
NXOpen.Point
) – StartNXOpen.Point
- endPoint (
NXOpen.Point
) – EndNXOpen.Point
Returns: Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
-------------------------------------
CreatePairedInfiniteLine¶
-
CurveCollection.
CreatePairedInfiniteLine
¶ Creates a paired
NXOpen.InfiniteLine
that is paired to the specified line.Signature
CreatePairedInfiniteLine(line)
Parameters: line ( NXOpen.Line
) – PairedNXOpen.Line
Returns: Return type: NXOpen.InfiniteLine
New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
CreateParabola¶
-
CurveCollection.
CreateParabola
¶ Overloaded method CreateParabola
CreateParabola(center, focalLength, minimumDY, maximumDY, rotationAngle, matrix)
CreateParabola(center, xDirection, yDirection, focalLength, minimumDY, maximumDY)
-------------------------------------
Creates a
NXOpen.Parabola
. The parabola will be created in a plane which passes through center and whose normal is the Z axis of the orientation matrix. (matrix.Element.xx, matrix.Element.xy, matrix.Element.xz) is the X axis of the orientation matrix. (matrix.Element.yx, matrix.Element.yy, matrix.Element.yz) is the Y axis of the orientation matrix. The rotation angle is measured relative to the X and Y axis of this orientation matrix.Signature
CreateParabola(center, focalLength, minimumDY, maximumDY, rotationAngle, matrix)
Parameters: - center (
NXOpen.Point3d
) – Center of parabola - focalLength (float) – Focal length
- minimumDY (float) – Minimum DY width
- maximumDY (float) – Maximum DY width
- rotationAngle (float) – Rotation angle in radians
- matrix (
NXOpen.NXMatrix
) – Orientation matrix for the parabola
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Parabola
. The parabola will be created through the origin and whose normal is Z axis.Signature
CreateParabola(center, xDirection, yDirection, focalLength, minimumDY, maximumDY)
Parameters: - center (
NXOpen.Point3d
) – Center of the parabola - xDirection (
NXOpen.Vector3d
) – X direction of the parabola - yDirection (
NXOpen.Vector3d
) – Y direction of the parabola - focalLength (float) – Focal length
- minimumDY (float) – Minimum DY width
- maximumDY (float) – Maximum DY width
Returns: Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateSmartCompositeCurve¶
-
CurveCollection.
CreateSmartCompositeCurve
¶ Overloaded method CreateSmartCompositeCurve
CreateSmartCompositeCurve(section, updateOption, tolerance)
CreateSmartCompositeCurve(curve, updateOption)
-------------------------------------
Creates a
NXOpen.Curve
. The smart composite curve will be created for the input section.Signature
CreateSmartCompositeCurve(section, updateOption, tolerance)
Parameters: - section (
NXOpen.Section
) – Section from which smart composite curve will be created - updateOption (
NXOpen.SmartObjectUpdateOption
) – - tolerance (float) – Tolerance used to join the section output curves
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a
NXOpen.Curve
. The smart composite curve will be created for the input curve.Signature
CreateSmartCompositeCurve(curve, updateOption)
Parameters: - curve (
NXOpen.Curve
) – Curve from which smart composite curve will be created - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateVirtualBlendCurve¶
-
CurveCollection.
CreateVirtualBlendCurve
¶ Creates a
NXOpen.Curve
.The virtual blend curve will be created for the input blend face. The virtual blend curve behaves similarly to the original edge that the blend face was applied on.
Signature
CreateVirtualBlendCurve(updateOption, blendFace, tolerance)
Parameters: - updateOption (
NXOpen.SmartObjectUpdateOption
) – - blendFace (
NXOpen.IParameterizedSurface
) – blend face - tolerance (float) – tolerance for computing the facsimile curve
Returns: Return type: New in version NX7.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- updateOption (
CreateVirtualCenterlineCurve¶
-
CurveCollection.
CreateVirtualCenterlineCurve
¶ Creates a
NXOpen.Curve
.The virtual centerline curve will be created for the input blend face.
Signature
CreateVirtualCenterlineCurve(updateOption, blendFace, tolerance)
Parameters: - updateOption (
NXOpen.SmartObjectUpdateOption
) – - blendFace (
NXOpen.IParameterizedSurface
) – blend face - tolerance (float) – tolerance for computing the facsimile curve
Returns: Return type: New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- updateOption (