ZLevelMillingBuilder Class¶
-
class
NXOpen.CAM.
ZLevelMillingBuilder
¶ Bases:
NXOpen.CAM.PlanarOperationBuilder
Represents a ZLevelMilling Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateZlevelMillingBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AdditionalPasses | Returns or sets the Boundary Additional Passes |
AutomaticPartBoundaryMethod | Returns or sets the Automatic Part Boundary Method |
BndStepover | Returns the boundary stepover builder |
ChannelName | Returns or sets the channel’s name |
CheckGeometry | Returns the check geometry builder |
CornerLoops | Returns or sets the corner loops value |
CutAreaGeometry | Returns the cut area geometry builder |
CutLevel | Returns the cut level builder |
CutParameters | Returns the cut parameter object |
CutPattern | Returns the cut pattern builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DeferCuttingStatus | Returns or sets the defer cutting status value |
DepthPerCut | Returns the depth per cut builder (inheritable double) |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MinCutLength | Returns the min cut length builder (tool dependent double) |
MotionOutput | Returns the motion output builder |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting moves builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PartGeometry | Returns the part geometry builder |
PathDisplayOptions | Returns the path display options builder |
ReferenceTool | Returns or sets the reference tool object |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolAxisFix | Returns the pmop tool axis ci builder |
ToolChangeSetting | Returns the tool change builder |
ToolMinimumLengthUsage | Returns or sets the tool minimum length usage |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
TrimBoundary | Returns the trim boundary |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CutLevel¶
-
ZLevelMillingBuilder.
CutLevel
¶ Returns the cut level builder
-------------------------------------
Getter Method
Signature
CutLevel()
Returns: the cut level builder Return type: NXOpen.CAM.CutLevel
New in version NX7.5.0.
License requirements: None.
TrimBoundary¶
-
ZLevelMillingBuilder.
TrimBoundary
¶ Returns the trim boundary
-------------------------------------
Getter Method
Signature
TrimBoundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ZLevelMillingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.