WedmOrientGeomBuilder Class¶
-
class
NXOpen.CAM.
WedmOrientGeomBuilder
¶ Bases:
NXOpen.CAM.OrientGeomBuilder
Represents a WedmOrientGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateWedmOrientGeomBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
FixtureOffsetBuilder | Returns the Fixture Offset builder |
LayoutCiBuilder | Returns the Save Layer/Layout builder |
LinkRcsToMcs | Returns or sets the link RCS to MCS |
Mcs | Returns or sets the MCS |
OptimizationMethod | Returns or sets the optim method |
Rcs | Returns or sets the RCS |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolAxisVector | Returns or sets the tool axis vector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCsysPurposeMode | Returns the CSYS purpose @return the CSYS purpose mode |
GetObject | Returns the object currently being edited by this builder. |
GetSpecialOutputMode | Returns the Special Output @return the special output mode |
GetToolAxisMode | Returns the tool axis mode @return the integer value |
SetCsysPurposeMode | Sets the CSYS purpose |
SetSpecialOutputMode | Sets the Special Output |
SetToolAxisMode | Sets the tool axis mode |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
WedmOrientGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.