WedmOperationBuilderInPathUdeSetTypes Enumeration¶
NXOpen.CAM.WedmOperationBuilder.InPathUdeSetTypes is an alias for NXOpen.CAM.WedmOperationBuilderInPathUdeSetTypes
-
class
NXOpen.CAM.
WedmOperationBuilderInPathUdeSetTypes
¶ Bases:
object
Represents the in path ude set type
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Start in path ude set at startEnd in path ude set at end-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-