WedmOperationBuilderBackburnPassesTypes Enumeration¶
NXOpen.CAM.WedmOperationBuilder.BackburnPassesTypes is an alias for NXOpen.CAM.WedmOperationBuilderBackburnPassesTypes
-
class
NXOpen.CAM.
WedmOperationBuilderBackburnPassesTypes
¶ Bases:
object
the types available for wedm backburn passes
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Single single backburn passMultipleRegionFirst multiple backburn passes - region firstMultipleCutoffFirst multiple backburn passes - cutoff first-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-