WedmCustomBoundaryDataBuilder Class¶
-
class
NXOpen.CAM.
WedmCustomBoundaryDataBuilder
¶ Bases:
NXOpen.Builder
Represents a WedmCustomBoundaryData Builder
No Creator
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
InpathEventDataList | Returns the inpath event data list |
TabPointList | Returns the tab point data list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateInpathEventDataBuilder | The create inpath event data builder @return inpath event data builder |
CreateTabPointDataBuilder | The create tab point data builder @return create tab point data builder |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InpathEventDataList¶
-
WedmCustomBoundaryDataBuilder.
InpathEventDataList
¶ Returns the inpath event data list
-------------------------------------
Getter Method
Signature
InpathEventDataList()
Returns: inpath event data list Return type: NXOpen.CAM.InPathEventDataBuilderList
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TabPointList¶
-
WedmCustomBoundaryDataBuilder.
TabPointList
¶ Returns the tab point data list
-------------------------------------
Getter Method
Signature
TabPointList()
Returns: tab point list Return type: NXOpen.CAM.TabPointDataBuilderList
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateInpathEventDataBuilder¶
-
WedmCustomBoundaryDataBuilder.
CreateInpathEventDataBuilder
¶ The create inpath event data builder
Signature
CreateInpathEventDataBuilder()
Returns: inpath event data builder Return type: NXOpen.CAM.InPathEventDataBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CreateTabPointDataBuilder¶
-
WedmCustomBoundaryDataBuilder.
CreateTabPointDataBuilder
¶ The create tab point data builder
Signature
CreateTabPointDataBuilder()
Returns: create tab point data builder Return type: NXOpen.CAM.TabPointDataBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
WedmCustomBoundaryDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.